FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Control wire of FR-HC RDY signal
FAQ
Control wire of FR-HC RDY signal
Is the contact between the terminals RDY and SE a NO contact or NC contact?
- Category :
Answer
The contact between the terminals RDY and SE is open collector output.
Operation is:
Normal: Non-conductive
Fault: Conductive
Operation is:
Normal: Non-conductive
Fault: Conductive
- Product Name
- Inverter, magnet motor drive
- Product Category
- High power factor converter
- Series
- Option