FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Relationship between frequency and output torque
FAQ
Relationship between frequency and output torque
When the frequency is changed by the FR-E520-0.4K, how the motor output torque change?
Do you have a graph for this relationship?
Do you have a graph for this relationship?
- Category :
Answer
The output torque characteristics of the FREQROL-E500 series are shown in the figure below. Figure 1
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E500