FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > FR-CV
FAQ
FR-CV
What is the proper use of the FR-CV and conventional FR-RC and FR-HC?
- Category :
Answer
Use the FR-HC to suppress harmonics. It also supports power supply regenerative driving.
The FR-CV and FR-RC are both power supply regeneration units.
The differences are:
The FR-CV allows for connecting multiple inverters. The FR-RC allows for connecting only one inverter.
The FR-CV can produce 100% regenerative torque with the same capacity as the inverter.
(The FR-RC can only produce 75% torque depending on the capacity.)
The FR-CV and FR-RC are both power supply regeneration units.
The differences are:
The FR-CV allows for connecting multiple inverters. The FR-RC allows for connecting only one inverter.
The FR-CV can produce 100% regenerative torque with the same capacity as the inverter.
(The FR-RC can only produce 75% torque depending on the capacity.)
- Product Name
- Inverter, magnet motor drive
- Product Category
- Power regeneration converter
- Series
- Option