FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > CC-Link
FAQ
CC-Link
While the FR-E520 has the CC-Link model, the FR-E540 does not have the CC-Link model according to the catalog.
When do you plan to have the 400 V class that supports CC-Link?
When do you plan to have the 400 V class that supports CC-Link?
- Category :
Answer
Already released.
Unlike the E520, you need to purchase the optional card FR-E5NC.
Unlike the E520, you need to purchase the optional card FR-E5NC.
- Product Name
- Inverter, magnet motor drive
- Series
- FR-E500