FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Installing frequency setting potentiometer
FAQ
Installing frequency setting potentiometer
Is it OK to install the frequency setting potentiometer WA2W 1 kΩ approximately 50 m apart from the inverter?
- Category :
Answer
When you are inputting analog signals, install the potentiometer within 30 m from the inverter.
(Refer to "Precaution on Selection and Operation" on the catalog.)
If the distance between the potentiometer and inverter is longer than this, the inverter may not operate normally due to voltage drop and noise.
(Refer to "Precaution on Selection and Operation" on the catalog.)
If the distance between the potentiometer and inverter is longer than this, the inverter may not operate normally due to voltage drop and noise.
- Product Name
- Inverter, magnet motor drive
- Series
- Others