FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Separation of operation panel
FAQ
Separation of operation panel
The operation panel of the E500 series can be removed and installed to another device with the back cover attached. Does S500 series also allow for separation of the operation panel?
- Category :
Answer
The operation panel of the FR-S500 is not detachable.
For the FR-S500-○○K-R (compatible with RS-485 communication), you can install the FR-PU04 on the enclosure surface by purchasing the FR-PU04 and PU cable.
For the FR-S500-○○K-R (compatible with RS-485 communication), you can install the FR-PU04 on the enclosure surface by purchasing the FR-PU04 and PU cable.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-S500