FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > All parameters returned to initial values
FAQ
All parameters returned to initial values
While using the A520, all parameters returned to the initial values.
What caused the A520 parameters to get initialized?
Are the A520 parameters backed up by a lithium battery? Or, is the EEPROM used?
What caused the A520 parameters to get initialized?
Are the A520 parameters backed up by a lithium battery? Or, is the EEPROM used?
- Category :
Answer
The parameters of the A500 series are stored in the EEPROM.
The reason why all parameters returned to the initial values is considered that you may have operated the inverter to clear the parameters by mistake.
The reason why all parameters returned to the initial values is considered that you may have operated the inverter to clear the parameters by mistake.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-A500