FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Thermal characteristics of motor
FAQ
Thermal characteristics of motor
While operating a three-phase motor with the same capacity as the FR-A500 (0.75 kW) under V/F control, the motor becomes too hot over continuous ON/OFF and gear change operations and the speed fluctuates within approximately 10 Hz range.
Please send a graph of relationship between the motor temperature and torque or speed precision, if any.
Please send a graph of relationship between the motor temperature and torque or speed precision, if any.
- Category :
Answer
Basically, when the motor temperature goes higher, the motor rotation speed goes lower.
The motor rotation speed also changes when the inverter input power supply state or load state changes.
Since relationship between the motor temperature and torque or speed precision depends on the motor used, contact the manufacturer of the motor.
The motor rotation speed also changes when the inverter input power supply state or load state changes.
Since relationship between the motor temperature and torque or speed precision depends on the motor used, contact the manufacturer of the motor.
- Product Name
- Inverter, magnet motor drive
- Series
- Others