FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Pulse frequency characteristics of terminal FM
FAQ
Pulse frequency characteristics of terminal FM
I want to display the frequency on a pulse input device such as a rotational HMI (Human Machine Interface).
- Category :
Answer
The terminal FM output pulse is directly proportional to the inverter output frequency.
With the initial setting, 1440 pulses/sec are output at 60 Hz (Pr.55), and up to 2400 pulses/sec can be output.
With the initial setting, 1440 pulses/sec are output at 60 Hz (Pr.55), and up to 2400 pulses/sec can be output.
- Product Name
- Inverter, magnet motor drive
- Series
- Others