FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Inverter
FAQ
Inverter
I want to acquire transition data of frequency and current value while a motor is operating with a motor. Do you have any good ideal (or product)?
Since the inverter is installed in the operation section, I cannot visually check them.
Since the inverter is installed in the operation section, I cannot visually check them.
- Category :
Answer
You can use the Hioki Memory HiCorder and clamp-on AC/DC high tester.
You can observe the inverter's frequency in one of the following two methods:
1. Attach the RC filter to the output from the terminals FM-SD.
2. Output from the terminals AM-5
(The terminal AM mentioned in 2. is only available with inverters equipped with the terminal AM, such as the FR-A500 series.)
Since you install the inverter in the operation section, the only recommended method is to install a Memory HiCorder in the operation section. (The inverter alone does not provide such a function.)
You can observe the inverter's frequency in one of the following two methods:
1. Attach the RC filter to the output from the terminals FM-SD.
2. Output from the terminals AM-5
(The terminal AM mentioned in 2. is only available with inverters equipped with the terminal AM, such as the FR-A500 series.)
Since you install the inverter in the operation section, the only recommended method is to install a Memory HiCorder in the operation section. (The inverter alone does not provide such a function.)
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E500, FR-A500