FAQ


FAQAbout Products
- FAQ > Drive Products > Inverters-FREQROL > Operation panel extension cable
FAQ
Operation panel extension cable
The specifications of the extension cable for the operation panel of the inverter E500 are same as the 10BASE-T (straight) LAN cable used to connect a hub and personal computer. Is this correct?
Can I use this type of cable within the limit of 20 m?
Can I use this type of cable within the limit of 20 m?
- Category :
Answer
Yes, you can use the 10BASE-T cable (straight) with the E500.
- Product Name
- Inverter, magnet motor drive
- Product Category
- Inverter
- Series
- FR-E500