FAQ


FAQAbout Products

- FAQ > Low-voltage Power Distribution Products > Power Management Meters > Electrical Indicators > Setting for communication (ME96SS series).
FAQ
Setting for communication (ME96SS series).
What items should be set for communication?
Answer
1) For the main body of ME96: Please set the following values on the “Set-up menu 2”.
In case of MODBUS RTU
In case of MODBUS RTU
|
Set-up menu No.
|
Setting items
|
Factory default settings
|
|||
SSHB
|
SSRB
|
SSEB
|
||||
(A)
|
2.2.
|
Address
|
1
|
|||
(B)
|
|
2.2.1.
|
Baud rate
|
19.2 kbps
|
||
(C)
|
|
2.2.2.
|
Parity
|
EVEn
|
||
(D)
|
|
2.2.3.
|
Stop bit
|
1
|
It is necessary that the settings of (B) to (D) mentioned above correspond to the settings of the upper system.
Please set the values so that there is no overlap of the address in the same system.
In case of MODBUS TCP
Please set the values so that there is no overlap of the address in the same system.
In case of MODBUS TCP
|
Set-up menu No.
|
Setting items
|
Factory default settings
|
||
SSHB
|
SSRB
|
SSEB
|
|||
(A)
|
2.4.
|
IP address
|
192.168.3.10
|
-
|
|
(B)
|
Sub-net mask
|
255.255.255.0
|
-
|
||
(C)
|
Use/non-use of a default gateway
|
oFF (Non-use)
|
-
|
||
(D)
|
Default gateway
|
127.0.0.1
|
-
|
In case of CC-Link
|
Set-up menu No.
|
Setting items
|
Factory default settings
|
|||
SSHB
|
SSRB
|
SSEB
|
||||
(A)
|
2.3.
|
Station No.
|
1
|
-
|
||
(B)
|
|
2.3.1.
|
Communication speed
|
156 kbps
|
-
|
|
(C)
|
|
2.3.2.
|
Communication version
|
1.10
|
-
|
In detail, please refer to the section 3 of the User’s Manual.
- Product Name
- Electronic Multi-Measuring Instrument
- Series
- ME96SS series