FAQ


FAQAbout Products
- FAQ > Low-voltage Power Distribution Products > Power Management Meters > Electrical Indicators > Active energy (lower digit indication) display upon communication test of MODBUS RTU/TCP communication (ME96SS series).
FAQ
Active energy (lower digit indication) display upon communication test of MODBUS RTU/TCP communication (ME96SS series).
When the active energy setting is set to 12-digit display on the communication test mode, how is the displayed value?
Answer
Regardless of setting, the value of the default digit length is replied.
When the register address “1304” for 6-digit display is set, the value varies with the full load.
As for the register address with a fixed unit, the value is displayed with 9-digit.
Register address for 9-digit display: “1309”, “1408” and “1426”
Register address for 9-digit display: “1309”, “1408” and “1426”
In detail, please refer to this category No.5.
- Product Name
- Electronic Multi-Measuring Instrument
- Series
- ME96SS series