FAQ
FAQAbout Products
- FAQ > Low-voltage Power Distribution Products > Power Management Meters > Electrical Indicators > Connectable number of MODBUS RTU (ME96SS series).
FAQ
Connectable number of MODBUS RTU (ME96SS series).
How many units can be connected to MODBUS RTU?
Is it possible to connect 64 units to MODBUS RTU using EMU4-SW1?
Is it possible to connect 64 units to MODBUS RTU using EMU4-SW1?
Answer
It is connectable with up to 31 units.
It is necessary to prepare at least 3 PCs for connecting with 64 units. (31 units + 31 units + 2 units)
It is necessary to prepare at least 3 PCs for connecting with 64 units. (31 units + 31 units + 2 units)
- Product Name
- Electronic Multi-Measuring Instrument
- Series
- ME96SS series
May I have your opinion?
Related FAQ
- Indication values of the main body is different from an obtained value through MODBUS RTU/ TCP (ME96SS series).
- Availability for battery exchange for Logging Unit (ME96SS series).
- Concurrent-use of MODBUS RTU and CC-Link.
- Replied value on the communication operation test of test mode (ME96SS series).
- LCD COM is flashing (ME96SS series).