FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Regarding MODBUS/TCP communication of the built-in Ethernet port
FAQ
Regarding MODBUS/TCP communication of the built-in Ethernet port
Does the built-in Ethernet port support MODBUS/TCP communication function?
Answer
When used as a master station, communication with a slave station can be performed using the simple CPU communication or the predefined protocol support function.
When using as a slave station, communicate with the master station can be performed by setting parameters.
In addition, one MELSEC iQ-F series module can be used as a slave and a master at the same time.
For the firmware and software versions of the supported CPU module, refer to the following manual.
MELSEC iQ-F FX5 User's Manual (MODBUS Communication)
When using as a slave station, communicate with the master station can be performed by setting parameters.
In addition, one MELSEC iQ-F series module can be used as a slave and a master at the same time.
For the firmware and software versions of the supported CPU module, refer to the following manual.
MELSEC iQ-F FX5 User's Manual (MODBUS Communication)
- Product Name
- FX5U, FX5UC, FX5UJ, FX5S
- Product Category
- CPU Module, Network/Communication
- Series
- MELSEC iQ-F Series