FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Regarding selection of FX3 intelligent function modules on the module configuration diagram of GX Works3
FAQ
Regarding selection of FX3 intelligent function modules on the module configuration diagram of GX Works3
Can the FX3 intelligent modules be selected on the module configuration diagram on GX Works3?
Answer
The FX3 intelligent function modules cannot be selected from the Element selection window because it does not correspond to the parameter setting of GX Works3. When using the FX3 intelligent function modules with the FX5U/FX5UC CPU modules, parameter settings must be handled programmatically.
For settings and programs, refer to the manual of dedicated FX3 intelligent function modles.
For settings and programs, refer to the manual of dedicated FX3 intelligent function modles.
- Product Name
- FX5U, FX5UC
- Product Category
- CPU Module, Engineering Software
- Series
- MELSEC iQ-F Series