FAQ


FAQAbout Products

- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Regarding the link refresh settings of FX5-CCL-MS
FAQ
Regarding the link refresh settings of FX5-CCL-MS
When setting the link refresh settings from GX Works3 by configuring the FX5-CCL-MS (CC-Link system master/intelligent device) as a master station, is it possible to use latch devices or I/O devices (X/Y) for link refresh devices?
- Category :
-
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > CPU Module
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Engineering Software
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Network/Communication
Answer
It is possible to use latch devices or I/O devices (X/Y) for link refresh devices.
However, when using I/O devices (X/Y), use I/O numbers (such as X1000 ~/Y1000~) that are not assigned to actual control.
Also, you can check the device allocation settings for refresh devices in GX Works3 by following the steps below.
View > Docking Window > Device Assignment Confirmation of GX Works3 menu and specify the appropriate module number in [Mounting Position No.].
However, make the network configuration settings and link refresh settings in the CC-Link parameters beforehand.
However, when using I/O devices (X/Y), use I/O numbers (such as X1000 ~/Y1000~) that are not assigned to actual control.
Also, you can check the device allocation settings for refresh devices in GX Works3 by following the steps below.
View > Docking Window > Device Assignment Confirmation of GX Works3 menu and specify the appropriate module number in [Mounting Position No.].
However, make the network configuration settings and link refresh settings in the CC-Link parameters beforehand.
- Product Name
- FX5-CCL-MS
- Product Category
- CPU Module, Network/Communication, Engineering Software
- Series
- MELSEC iQ-F Series