FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > Regarding the frequency of high-speed counters
FAQ
Regarding the frequency of high-speed counters
Which frequencies can be used for the FX5 CPU high-speed counters?
Answer
The maximum frequency of the FX5U/FX5UC CPU module is 200kHz and the maximum frequency of the FX5S/FX5UJ CPU module is 100 kHz.
- Product Name
- FX5U, FX5UC, FX5UJ, FX5S
- Product Category
- CPU Module, High-Speed Counter
- Series
- MELSEC iQ-F Series