FAQ
FAQAbout Products
- FAQ > Low-voltage Power Distribution Products > Low-voltage Circuit Breakers > Accessories and Related Components > AL/AX direct connection to PLC
FAQ
AL/AX direct connection to PLC
Is it possible to input AL and AX switch directly to PLCs?
Answer
It is necessary to use AL and AX switches that are suitable for the specification of
PLC input unit. Generally AL and AX switch for micro-load are used for it. Moreover, since chattering may occur for the AL and AX switches of circuit breaker within several milli-seconds for switching, please consider the input setting at PLC side that is input-detected again about 10ms later after input detection.
PLC input unit. Generally AL and AX switch for micro-load are used for it. Moreover, since chattering may occur for the AL and AX switches of circuit breaker within several milli-seconds for switching, please consider the input setting at PLC side that is input-detected again about 10ms later after input detection.
- Product Name
- Internal Accessories
- Series
- WS-V