Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • No : 22400
  • Release Date : 2018/08/31 14:33
  • Print

Side by side installation

Is it possible that MCCBs or ELCBs are closely installed?
Category : 

Answer

It is possible to attach closely if there is no problem about the insulation distance between live parts such as a terminal bar and load currents are 80% or less than the rated current.
Product Name
Molded Case Circuit Breakers
Series
WS-V

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries