Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 22438
  • Release Date : 2018/08/31 14:33
  • Print

Default setting of electronic breakers

What is the default set value of an overcurrent characteristic setting knob of an electronic circuit breaker when shipping?
Category : 

Answer

Each setting knob of the overcurrent trip characteristic is set to the maximum value and then shipped if not specified. However, only the pre-alarm is set to the minimum value (70%).
Product Name
Molded Case Circuit Breakers
Series
WS-V

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries