FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-R Series > Overhead time of when a fixed scan execution type program of the MELSEC iQ-R series CPU module is executed
FAQ
Overhead time of when a fixed scan execution type program of the MELSEC iQ-R series CPU module is executed
How long is the overhead time of when a fixed scan execution type program of the MELSEC iQ-R series CPU module?
- Category :
Answer
When the block number of the file register (R) is saved and stored, the overhead time becomes 35.9 [us].
When the number of the file register is not saved or stored, the overhead time becomes 18.6 [us].
When the number of the file register is not saved or stored, the overhead time becomes 18.6 [us].
- Product Name
- MELSEC iQ-R Series
- Series
- MELSEC iQ-R Series