FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-R Series > Number of modules that can be synchronized using the MELSEC iQ-R series inter-module synchronization function
FAQ
Number of modules that can be synchronized using the MELSEC iQ-R series inter-module synchronization function
How may modules can be synchronized using the MELSEC iQ-R series inter-module synchronization function?
- Category :
Answer
The number of modules that can be synchronized is as follows.
- In single CPU system configuration: 64 modules
- In multiple CPU system configuration: 57 to 63 modules
Mounting positions of the modules and the maximum number of mountable modules do not change regardless of whether
the inter-module synchronization function is used or not.
Since RnENCPU occupies two slots, one or more slots are occupied, so the maximum number of installable modules decreases.
- In single CPU system configuration: 64 modules
- In multiple CPU system configuration: 57 to 63 modules
Mounting positions of the modules and the maximum number of mountable modules do not change regardless of whether
the inter-module synchronization function is used or not.
Since RnENCPU occupies two slots, one or more slots are occupied, so the maximum number of installable modules decreases.
- Product Name
- MELSEC iQ-R Series
- Series
- MELSEC iQ-R Series