FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-L Series > CPU built-in I/O function
FAQ
CPU built-in I/O function
Can I use the CPU built-in high-speed counter function and positioning function simultaneously?
- Category :
Answer
They can be used simultaneously when I/O signals are not overlapped. The overlap of signals are checked automatically when a user select functions in the built-in I/O function parameter setting window.
- Product Name
- MELSEC-L Series
- Series
- CPU