FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > Engineering Software > Accessing a QnA compatible Ethernet interface module via a router using GX Developer
FAQ
Accessing a QnA compatible Ethernet interface module via a router using GX Developer
Is it possible to connect GX Developer to a QnA compatible Ethernet interface module via a router using the Ethernet adapter on the personal computer?
- Category :
Answer
For GX Developer, a connection via a QnA compatible Ethernet interface module allows communication only within the same segment. Via a router, it is impossible to access programmable controller CPU modules within other segments via a For QnA Ethernet interface module.
- Product Name
- Engineering Software
- Series
- Software Package (GPP function)