FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > Engineering Software > Limit on the display of data collected in GX LogViewer to 32 values
FAQ
Limit on the display of data collected in GX LogViewer to 32 values
There are more than 32 collected data values in GX LogViewer. The setting of display is limited to 32 values at maximum. Why is the display limited?
- Category :
Answer
GX LogViewer is made to a specification that allows a single trend window to display a maximum of 32 graphs. When there are more than 32 logging data values, select [Graph View] -> [Change the Data to Draw Graphs] from the menu to display the rest.
- Product Name
- Engineering Software
- Series
- Software Package (other functions)