FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > Engineering Software > Necessity for GX Configurator-SC
FAQ
Necessity for GX Configurator-SC
Is GX Configurator-SC required for a serial communication module to be used?
- Category :
Answer
The serial communication modules do not require GX Configurator-SC.
However, we recommend GX Configurator-SC as it reduces man-hours.
(1) The predefined protocol support function makes it easy to set the protocol necessary to communicate with a target device
such as a temperature control module and a barcode reader.
(2) The debug support function can be used to:
- trace the status of send/receive packets and signal lines using the circuit trace function.
- monitor the error state of the module and signal lines using the state monitor function.
However, we recommend GX Configurator-SC as it reduces man-hours.
(1) The predefined protocol support function makes it easy to set the protocol necessary to communicate with a target device
such as a temperature control module and a barcode reader.
(2) The debug support function can be used to:
- trace the status of send/receive packets and signal lines using the circuit trace function.
- monitor the error state of the module and signal lines using the state monitor function.
- Product Name
- Engineering Software
- Series
- Software Package (other functions)