FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > Engineering Software > An error (error code: F1028) occurs when compilation is executed in GX Works2.
FAQ
An error (error code: F1028) occurs when compilation is executed in GX Works2.
I have created a program "with labels" with GX Works2, and an error (error code: F1028) occurs when I execute compilation (conversion).
- Category :
Answer
You have used the device set as the automatic assignment device for labels in the program. Change the device with the one out of the range or change the automatic assignment device range.
- Product Name
- Engineering Software
- Series
- GX Works2