FAQ


FAQAbout Products

- FAQ > Controllers > Programmable Controllers MELSEC > Network related products > T-branch connection and star topology for CC-Link networks
FAQ
T-branch connection and star topology for CC-Link networks
What are a CC-Link T-branch connection and a star topology?
- Category :
Answer
- T-branch
T-branch is a connection type that branches one line from a main line.
To establish a T-branch CC-Link network, use the repeater module AJ65SBT-RPT or branching terminals with no repeater module.
- Star topology
A star topology is a connection type that branches multiple communication lines radially from one branch point.
To establish a star topology CC-Link network, use the low profile waterproof type repeater hub module AJ65FBTA-RPH or
spring clamp terminal block type repeater hub module AJ65BTS-RPH.
T-branch is a connection type that branches one line from a main line.
To establish a T-branch CC-Link network, use the repeater module AJ65SBT-RPT or branching terminals with no repeater module.
- Star topology
A star topology is a connection type that branches multiple communication lines radially from one branch point.
To establish a star topology CC-Link network, use the low profile waterproof type repeater hub module AJ65FBTA-RPH or
spring clamp terminal block type repeater hub module AJ65BTS-RPH.
- Product Name
- Network Related Products
- Series
- CC-Link