Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 23319
  • Release Date : 2018/09/12 15:11
  • Print

About Low-voltage Power Distribution Products

Is it possible to produce SR-T* and SRD-T* type including a surgesuppressor?
Category : 

Answer

It is possible to produce with the coil designation of less than AC 230V andDC 220V. Please add " SA" at the end of the type name.
Product Name
Motor Starters
Series
MS-T/N

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries