FAQ


FAQAbout Products
- FAQ > Low-voltage Power Distribution Products > Contactors and Motor Starters > Motor Starters > About Low-voltage Power Distribution Products
FAQ
About Low-voltage Power Distribution Products
What is the temperature of US-N* type cooling fins when carryingthe rated current?
Answer
When carrying the rated current at ambient temperature of 40℃ (whencarrying the rated heater load), the maximum temparature of cooling finis approximately 100℃.
- Product Name
- Motor Starters
- Series
- MS-T/N