FAQ


FAQAbout Products

- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > Differences in the panel cutting dimensions from the GOT1000 series
FAQ
Differences in the panel cutting dimensions from the GOT1000 series
Do the GOT1000 series and GOT2000 series have the same panel cutting dimensions when their models are the same in screen sizes?
- Category :
-
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT27
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT25
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT21
Answer
The GOT1000 series and GOT2000 series have the same panel cutting dimensions when their models are the same in screen sizes (excluding the GT25 open frame model).
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- GOT
- Series
- GOT2000 Series