FAQ


FAQAbout Products
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > Compatibility of communication cables for the GOT1000 series
FAQ
Compatibility of communication cables for the GOT1000 series
Can the communication cables for the GOT1000 series be used for the GOT2000 series?
- Category :
-
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT27
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT25
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT21
Answer
Only when the connectors have the same number of pins, shape, and communication format, the communication cable for the GOT1000 series can be used for the GOT2000 series as well.
The following communication cables for the GOT1000 series cannot be used for the GOT2000 series.
■ For GT16
・ GT16-C02RS-9S
・ GT16-C02RS-25S
・ FA-LTBGTR4CBL05
・ FA-LTBGTR4CBL10
・ FA-LTBGTR4CBL20
■ For GT10
・ GT10-RS2TUSB-5S
The following communication cables for the GOT1000 series cannot be used for the GOT2000 series.
■ For GT16
・ GT16-C02RS-9S
・ GT16-C02RS-25S
・ FA-LTBGTR4CBL05
・ FA-LTBGTR4CBL10
・ FA-LTBGTR4CBL20
■ For GT10
・ GT10-RS2TUSB-5S
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- Cable
- Series
- GOT2000 Series