Start main contents

Factory Automation

  • Font Size
  • S
  • M
  • L

Questions

  • No : 23433
  • Release Date : 2018/09/14 15:06
  • Update : 2018/09/26 16:47
  • Print

Compatibility of the option board for the MES interface function

Can the option board for the MES interface function for the GOT1000 series be used for the GOT2000 series?
Category : 

Answer

The option board for the MES interface function for the GOT1000 series (GT16-MESB/GT15-MESB48M) cannot be used for the GOT2000 series.

Use the license of the MES interface function for the GOT2000 series (GT25-MESIFKEY).
In addition, when the BootOS version of the GOT is "C" or earlier, updating the BootOS version to "D" or later is required.


* To update the BootOS version to "D" or later, GT Designer3 (GOT2000) Version1.108N or later is required.

For information on how to update (install) the BootOS, refer to the following.
・ GT Designer3 (GOT2000) Screen Design Manual (SH-081220ENG)
 "4.3.2 Transferring data" or
 "4.5.3 Installing the BootOS or the CoreOS to the GOT"
Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
Option (option function board), GOT function (MES interface)
Series
GOT2000 Series
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?