FAQ


FAQAbout Products
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > Using with the GOT1000 series in the client/server function
FAQ
Using with the GOT1000 series in the client/server function
Can a GOT1000 series model and a GOT2000 series model be used together on a client/server of the gateway function?
Answer
A GOT1000 series model and a GOT2000 series model can be used together on a client/server of the gateway function.
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- GOT function (gateway)
- Series
- GOT2000 Series