FAQ


FAQAbout Products
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > Wireless LAN communication unit and wireless LAN access point
FAQ
Wireless LAN communication unit and wireless LAN access point
Can the wireless LAN communication unit (GT25-WLAN) be used as an access point?
Answer
The wireless LAN communication unit (GT25-WLAN) can be used as an access point.
* Compatible with GT Designer3 (GOT2000) Version1.144A or later.
Use the BootOS version "C" or later.
* Up to five stations are connectable.
* The standards, which must be complied with by the countries where the unit can be used, differ depending on the hardware version of the wireless LAN communication unit (GT25-WLAN).
For the details, refer to the following Technical News.
・ GOT2000 Series Wireless LAN Communication Unit (GT25-WLAN) Complies with Overseas Radio Laws and Regulations (GOT-A-0096)
* Compatible with GT Designer3 (GOT2000) Version1.144A or later.
Use the BootOS version "C" or later.
* Up to five stations are connectable.
* The standards, which must be complied with by the countries where the unit can be used, differ depending on the hardware version of the wireless LAN communication unit (GT25-WLAN).
For the details, refer to the following Technical News.
・ GOT2000 Series Wireless LAN Communication Unit (GT25-WLAN) Complies with Overseas Radio Laws and Regulations (GOT-A-0096)
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- Communication unit
- Series
- GOT2000 Series