FAQ


FAQAbout Products
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > Connecting FA devices through the wireless LAN communication unit (GT25-WLAN)
FAQ
Connecting FA devices through the wireless LAN communication unit (GT25-WLAN)
Can an FA device such as a PLC and the GOT be connected through a wireless LAN by using the wireless LAN communication unit (GT25-WLAN)?
Answer
An FA device such as a PLC and the GOT cannot be connected through a wireless LAN by using the wireless LAN communication unit (GT25-WLAN).
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- Communication unit, GOT function (communication)
- Series
- GOT2000 Series