FAQ


FAQAbout Products

- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > How to use the wireless LAN communication unit (GT25-WLAN)
FAQ
How to use the wireless LAN communication unit (GT25-WLAN)
What is the wireless LAN communication unit (GT25-WLAN) used for?
Answer
The following functions are available with the wireless LAN connection by using the wireless LAN communication unit (GT25-WLAN).
・ Communication with GT Designer3
・ FA transparent function
・ Time setting function (Acquiring time-of-day information from the SNTP server)
・ Remote personal computer operation (Ethernet) function
・ VNC server function
・ Multimedia function (Sending a video file to a personal computer)
・ Server function, client function
・ Mail send function
・ FTP server function
・ File transfer function (FTP transfer)
・ SoftGOT-GOT link function
・ MES interface function
・ Log viewer function
・ GOT Mobile function
* The standards, which must be complied with by the countries where the unit can be used, differ depending on the hardware version of the wireless LAN communication unit (GT25-WLAN).
For the details, refer to the following Technical News.
・ GOT2000 Series Wireless LAN Communication Unit (GT25-WLAN) Complies with Overseas Radio Laws and Regulations (GOT-A-0096)
For information on how to use the wireless LAN communication unit (GT25-WLAN), refer to the following.
・ GT Designer3 (GOT2000) Screen Design Manual (SH-081220ENG)
"5.3.12 Configuring the settings for a wireless LAN ([Wireless LAN Setting])"
・ Communication with GT Designer3
・ FA transparent function
・ Time setting function (Acquiring time-of-day information from the SNTP server)
・ Remote personal computer operation (Ethernet) function
・ VNC server function
・ Multimedia function (Sending a video file to a personal computer)
・ Server function, client function
・ Mail send function
・ FTP server function
・ File transfer function (FTP transfer)
・ SoftGOT-GOT link function
・ MES interface function
・ Log viewer function
・ GOT Mobile function
* The standards, which must be complied with by the countries where the unit can be used, differ depending on the hardware version of the wireless LAN communication unit (GT25-WLAN).
For the details, refer to the following Technical News.
・ GOT2000 Series Wireless LAN Communication Unit (GT25-WLAN) Complies with Overseas Radio Laws and Regulations (GOT-A-0096)
For information on how to use the wireless LAN communication unit (GT25-WLAN), refer to the following.
・ GT Designer3 (GOT2000) Screen Design Manual (SH-081220ENG)
"5.3.12 Configuring the settings for a wireless LAN ([Wireless LAN Setting])"
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- Communication unit
- Series
- GOT2000 Series