FAQ
FAQAbout Products
- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > Ethernet connection between GT SoftGOT2000 and a PLC
FAQ
Ethernet connection between GT SoftGOT2000 and a PLC
I want to connect GT SoftGOT2000 and a QnUDVCPU by Ethernet by using the Ethernet port built in the CPU.
How can I set it?
How can I set it?
Answer
The following describes an example of settings to connect GT SoftGOT2000 and the Ethernet port built in the QnUDVCPU by Ethernet.
1. Configure the following settings in GT Designer3 (GOT2000).
◆ For GT Designer3 (GOT2000) Version1.100E or later
(1) Select [Common] → [Controller Setting] → [CH1] from the menu.
Manufacturer: MITSUBISHI ELECTRIC
Controller Type: MELSEC-Q/QS, Q17nD/M/NC/DR, CRnD-700
(2) Select [Common] → [Controller Setting] → [CH1] → [Connected Ethernet Controller Setting] (or [Ethernet Controller Setting]) from the menu.
Host: *
Net No.: 1 (example)
Station: 1 (example)
Unit Type: QnUD(P)V/QnUDE(H)
IP address 192.168.3.39
Port No. 5006
Communication: UDP
2. Configure the following settings in GT SoftGOT2000 Version1.
(1) Select [Online] → [Communication Setup] → [Connection Setup] from the menu.
Connection: Ethernet
Type: MITSUBISHI ELECTRIC (or MELSEC)
Net No.: 1
PC No.: 3
Port No.: 5001
3. Configure the following settings in GX Works2.
(1) Select [Parameter] → [PLC parameter] → [Built-in Ethernet Port Setting] from the menu.
IP address: 192.168.3.39
Subnet Mask Pattern: 255.255.255.0
(2) Select [Parameter] → [PLC parameter] → [Built-in Ethernet Port Setting] → [Open Setting] from the menu.
Protocol: UDP
Open System: MELSOFT Connection
For the details, refer to the following.
• GT SoftGOT2000 Version1 Operating Manual (SH-081201ENG-AB)
"3.6.4 Controller setting"
1. Configure the following settings in GT Designer3 (GOT2000).
◆ For GT Designer3 (GOT2000) Version1.100E or later
(1) Select [Common] → [Controller Setting] → [CH1] from the menu.
Manufacturer: MITSUBISHI ELECTRIC
Controller Type: MELSEC-Q/QS, Q17nD/M/NC/DR, CRnD-700
(2) Select [Common] → [Controller Setting] → [CH1] → [Connected Ethernet Controller Setting] (or [Ethernet Controller Setting]) from the menu.
Host: *
Net No.: 1 (example)
Station: 1 (example)
Unit Type: QnUD(P)V/QnUDE(H)
IP address 192.168.3.39
Port No. 5006
Communication: UDP
2. Configure the following settings in GT SoftGOT2000 Version1.
(1) Select [Online] → [Communication Setup] → [Connection Setup] from the menu.
Connection: Ethernet
Type: MITSUBISHI ELECTRIC (or MELSEC)
Net No.: 1
PC No.: 3
Port No.: 5001
3. Configure the following settings in GX Works2.
(1) Select [Parameter] → [PLC parameter] → [Built-in Ethernet Port Setting] from the menu.
IP address: 192.168.3.39
Subnet Mask Pattern: 255.255.255.0
(2) Select [Parameter] → [PLC parameter] → [Built-in Ethernet Port Setting] → [Open Setting] from the menu.
Protocol: UDP
Open System: MELSOFT Connection
For the details, refer to the following.
• GT SoftGOT2000 Version1 Operating Manual (SH-081201ENG-AB)
"3.6.4 Controller setting"
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- GT SoftGOT2000
- Series
- GOT2000 Series