FAQ


FAQAbout Products

- FAQ > Human Machine Interfaces > Human-Machine Interfaces(HMIs)-GOT > GOT2000 Series > Procedure to use the screen gesture function
FAQ
Procedure to use the screen gesture function
How can I start to use the screen gesture function?
Answer
Perform the following procedure to use the screen gesture function.
◆ GT Designer3 (GOT2000) Version 1.100E or later
1. Select [Common] - [GOT Type Setting]. Select [Use the gesture function], and click [OK].
2. Place a key code switch (screen gesture mode switching) to switch between the screen gesture mode and normal operation mode in the screen gesture inactive area (a 32-dot area from the top edge of the screen).
3. Touch the key code switch (screen gesture mode switching) placed on the base screen of the GOT.
To display the screen gesture inactive area on the drawing screen, select [Screen] - [Screen Property]. Then, select [Display the screen gesture inactive area], and click [OK].
In addition, to make the drawing process smoother, select [Common] - [GOT Type Setting], and then select [Enable the graphics accelerator].
This setting is available for the following conditions.
GT Designer3 (GOT2000) Version 1.185T or later and GOT Graphic Ver.1, or GT Designer3 (GOT2000) Version 1.112S or later and 1.181P or earlier
Note that the following restrictions are applied.
・ GOT startup may become slower.
・ In the screen gesture mode, the object display is not refreshed.
◆ GT Designer3 (GOT2000) Version 1.100E or later
1. Select [Common] - [GOT Type Setting]. Select [Use the gesture function], and click [OK].
2. Place a key code switch (screen gesture mode switching) to switch between the screen gesture mode and normal operation mode in the screen gesture inactive area (a 32-dot area from the top edge of the screen).
3. Touch the key code switch (screen gesture mode switching) placed on the base screen of the GOT.
To display the screen gesture inactive area on the drawing screen, select [Screen] - [Screen Property]. Then, select [Display the screen gesture inactive area], and click [OK].
In addition, to make the drawing process smoother, select [Common] - [GOT Type Setting], and then select [Enable the graphics accelerator].
This setting is available for the following conditions.
GT Designer3 (GOT2000) Version 1.185T or later and GOT Graphic Ver.1, or GT Designer3 (GOT2000) Version 1.112S or later and 1.181P or earlier
Note that the following restrictions are applied.
・ GOT startup may become slower.
・ In the screen gesture mode, the object display is not refreshed.
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- GOT function (gesture)
- Series
- GOT2000 Series