Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 23459
  • Release Date : 2018/09/14 15:06
  • Update : 2025/10/09 18:02
  • Print

Disabling the screen gesture function

Answer

The following shows how to disable the screen gesture function.

◆ For GT Designer3 (GOT2000) Version 1
Select [Common] → [GOT Type Setting], deselect [Use the gesture function] and click [OK].

* The above setting also disables the object gesture function. 
* For the GOT3000 series, only models with a capacitive-type touch panel are compatible with screen gesture mode.

Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
GOT function (gesture)
Series
GOT2000 Series, GOT3000 Series

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries