FAQ


FAQAbout Products
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > Object gesture function while using the GOT remote access function
FAQ
Object gesture function while using the GOT remote access function
Can I use the object gesture function from the VNC client while using the GOT remote access function (VNC server function)?
- Category :
-
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT27
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT3000 Series
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT3000 Series > GT37
Answer
You cannot use the object gesture function from the VNC client while using the GOT remote access function (VNC server function).
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- GOT function (gesture), GOT function (VNC server)
- Series
- GOT2000 Series, GOT3000 Series