Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 23471
  • Release Date : 2018/09/14 15:06
  • Update : 2025/10/09 18:12
  • Print

Scrolling with the screen gesture function

Can I display an object placed in the temporary area of the base screen while creating a screen on the GOT with scroll operations in screen gesture mode?

Category : 

Answer

You cannot display any object placed in the temporary area of the base screen while creating a screen on the GOT with scroll operations in screen gesture mode.

* For the GOT3000 series, only models with a capacitive-type touch panel are compatible with screen gesture mode.

Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
GOT function (gesture)
Series
GOT2000 Series, GOT3000 Series

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries