Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 23481
  • Release Date : 2018/09/14 15:06
  • Update : 2025/10/09 18:35
  • Print

Touching the screen gesture active area

Answer

You cannot touch the switches in the screen gesture active area in screen gesture mode. 
To touch the switches, disable screen gesture mode by touching either of the following switches placed outside the screen gesture active area.

• The screen gesture mode switch (key code: FF90)
• The full scale display (100% display) switch (key code: FF91)

* For the GOT3000 series, only models with a capacitive-type touch panel are compatible with screen gesture mode.

Product Name
Human-Machine Interfaces(HMIs)-GOT
Product Category
GOT function (gesture)
Series
GOT2000 Series, GOT3000 Series

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries