FAQ


FAQAbout Products

- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > Touching the screen gesture active area
FAQ
Touching the screen gesture active area
How can I touch the switches placed in the screen gesture active area in the screen gesture mode?
Answer
You cannot touch the switches in the screen gesture active area in the screen gesture mode.
To be able to touch the switches, touch either of the following switches placed outside the screen gesture active area to cancel the screen gesture mode.
・ Screen gesture mode selector switch (key code: FF90)
・ Full scale display (100%) switch (key code: FF91)
* The full scale display (100%) switch is supported by GT Designer3 (GOT2000) Version 1.105K or later.
To be able to touch the switches, touch either of the following switches placed outside the screen gesture active area to cancel the screen gesture mode.
・ Screen gesture mode selector switch (key code: FF90)
・ Full scale display (100%) switch (key code: FF91)
* The full scale display (100%) switch is supported by GT Designer3 (GOT2000) Version 1.105K or later.
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- GOT function (gesture)
- Series
- GOT2000 Series