FAQ


FAQAbout Products
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > Checking screen gesture mode
FAQ
Checking screen gesture mode
Can I check that screen gesture mode is enabled on the screen?
- Category :
-
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT27
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT3000 Series
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT3000 Series > GT37
Answer
When screen gesture mode is enabled, a frame indicating the screen gesture active area is displayed.
This frame is displayed with a bright red line only when the contents within the screen gesture active area are not enlarged, and with a combination of bright red and dark red lines when the contents are enlarged. You can check that screen gesture mode is enabled when this frame is displayed.

* For the GOT3000 series, only models with a capacitive-type touch panel are compatible with screen gesture mode.
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- GOT function (gesture)
- Series
- GOT2000 Series, GOT3000 Series