FAQ


FAQAbout Products
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > Transferring data between a personal computer and a GOT via a PLC
FAQ
Transferring data between a personal computer and a GOT via a PLC
Can the GOT screen data be read and written from and to a personal computer via a PLC?
- Category :
-
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT27
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT25
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT3000 Series
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT3000 Series > GT37
Answer
The GOT screen data can be read and written from and to a personal computer via a PLC.
Note that the following items have restrictions.
• Connection type between the personal computer and the PLC
• Connection type between the PLC and the GOT
• Relay PLC type
• Screen design software version
The following items have restrictions depending on the relay PLC type.
• Serial number of the PLC
• PLC engineering software version
For details, refer to the screen design software manual.

- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- GOT function (screen data transfer)
- Series
- GOT3000 Series, GOT2000 Series