FAQ


FAQAbout Products

- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > Necessity of the UV protective sheet for the rugged model
FAQ
Necessity of the UV protective sheet for the rugged model
Is the UV protective sheet necessary for improving the UV protection for the rugged model?
Answer
The UV protective sheet (option) is not necessary for improving the UV protection for the rugged model.
Without the UV protective sheet, the rugged model is more resistant to UV than any other GOT models.
If the rugged model is exposed to UV for a long period, the GOT front face may turn yellow.
Attaching the UV protective sheet improves UV cutoff and prevents the environmental protection sheet (not replaceable) on the GOT front face from fading in color.
Without the UV protective sheet, the rugged model is more resistant to UV than any other GOT models.
If the rugged model is exposed to UV for a long period, the GOT front face may turn yellow.
Attaching the UV protective sheet improves UV cutoff and prevents the environmental protection sheet (not replaceable) on the GOT front face from fading in color.
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- Rugged model, option (UV protective sheet)
- Series
- GOT2000 Series