FAQ


FAQAbout Products
- FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > GT25 Rugged > Optional UV protective sheet for the rugged model
FAQ
Optional UV protective sheet for the rugged model
When the optional UV protective sheet for the rugged model is attached, how much is the UV cutoff?
Answer
When the optional UV protective sheet for the rugged model is attached, 99.75% of UV is cut off.
・ When the protective cover for oil is used: 0.05 × 1 = 0.05 (95% cutoff)
・ When the UV protective sheet is used: 0.05 × 0.05 = 0.0025 (99.75% cutoff)
・ When the protective cover for oil is used: 0.05 × 1 = 0.05 (95% cutoff)
・ When the UV protective sheet is used: 0.05 × 0.05 = 0.0025 (99.75% cutoff)
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- Rugged model, option (UV protective sheet)
- Series
- GOT2000 Series