FAQ


FAQAbout Products
 
 - FAQ > Human Machine Interfaces > Human Machine Interfaces MELHMI-GOT > GOT2000 Series > Location of the terminating resistor setting switch for the RS-422/485 communication port
FAQ
Location of the terminating resistor setting switch for the RS-422/485 communication port
      Where is the terminating resistor setting switch for the RS-422/485 communication port located on the rugged model?
    
  
Answer
    The terminating resistor setting switch for the RS-422/485 communication port is located inside the battery cover on the back of the rugged model. 
For the details, refer to the following.
GOT2000 Series User's Manual (Hardware) (SH(NA)-081194ENG-X)
"4.3 GT2507T-W"
    For the details, refer to the following.
GOT2000 Series User's Manual (Hardware) (SH(NA)-081194ENG-X)
"4.3 GT2507T-W"
- Product Name
- Human-Machine Interfaces(HMIs)-GOT
- Product Category
- Rugged model
- Series
- GOT2000 Series